Hello,
I trying to run the pingpong example on the Sabre SD board with iMX6Solox. I have been able to build and boot core-image-minimal and core-image-base using the 3.10.53 BSP. The problem is that both of them do not have the pingpong example capabilities.
I used the following:
1. MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build
2. bitbake core-image-base
So i tried with 3.14.52 and 4.1.15, they both have the pingpong code in them but do not boot for me on the same board. Not booting is usually looping on "Starting Kernel....".
I followed the instruction to the letter and i guess i am missing something. If i want to build the "base" image with no graphical backend, which DISTRO should i use and how exactly do i need to configure the build?
This is what i see on the terminal when it loops:
U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Aug 08 2016 - 23:27:21)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 34 C
Reset cause: POR
Board: MX6SX SABRE SDB
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
Display: Hannstar-XGA (1024x768)
Video: 1024x768x18
gis input --- No input
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc2 is current device
switch to partitions #0, OK
mmc2 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6037600 bytes read in 377 ms (15.3 MiB/s)
Booting from mmc ...
reading imx6sx-sdb.dtb
47342 bytes read in 18 ms (2.5 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5c2060 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300e8ed
switch to ldo_bypass mode!
Starting kernel ...
U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Aug 08 2016 - 23:27:21)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 38 C
Reset cause: POR
Board: MX6SX SABRE SDB
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
Display: Hannstar-XGA (1024x768)
Video: 1024x768x18
gis input --- No input
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc2 is current device
switch to partitions #0, OK
mmc2 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6037600 bytes read in 377 ms (15.3 MiB/s)
Booting from mmc ...
reading imx6sx-sdb.dtb
47342 bytes read in 18 ms (2.5 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5c2060 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300e8ed
switch to ldo_bypass mode!
Starting kernel ...
U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Aug 08 2016 - 23:27:21)
CPU: Freescale i.MX6SX rev1.2 at 792 MHz
CPU: Temperature 39 C
Reset cause: POR
Board: MX6SX SABRE SDB
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x11
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
*** Warning - bad CRC, using default environment
Display: Hannstar-XGA (1024x768)
Video: 1024x768x18
gis input --- No input
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2 is current device
Net: FEC [PRIME]
Normal Boot
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc2 is current device
switch to partitions #0, OK
mmc2 is current device
reading boot.scr
** Unable to read file boot.scr **
reading zImage
6037600 bytes read in 378 ms (15.2 MiB/s)
Booting from mmc ...
reading imx6sx-sdb.dtb
47342 bytes read in 18 ms (2.5 MiB/s)
Kernel image @ 0x80800000 [ 0x000000 - 0x5c2060 ]
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300e8ed
switch to ldo_bypass mode!
Starting kernel ...
Thanks,
Evgeny