iMX6quad SABRE SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6quad SABRE SDB

808 Views
basinibharathi
Contributor II

Hi,

I am working on iMX6 quad sabre sd board booting with android OS(SD Card). I want to implement some applications related to image processing, video/audio processing using existing interfaces/peripherals.

Which is the right platform/software to write the code for the application and integrate the same with the existing OS on the iMX6 and debug/test the same.

Please suggest me on the above.

Thanks,

Bharathi

Labels (1)
3 Replies

715 Views
art
NXP Employee
NXP Employee

This is a kind of general Android application development question. So, please refer to the following resource:

https://developer.android.com/index.html


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

715 Views
basinibharathi
Contributor II

Hi Artur,

Thanks for your input.

When I tried to install a new apk file on my SD card and boot iMX6, I am not seeing the application on HDMI screen, even though the application is installed successfully using the below command.

adb install application.apk

Any idea what could be the wrong?

Regards,

Bharathi

0 Kudos

715 Views
basinibharathi
Contributor II

Also, Can Android Studio supports 'C ' language or only java ? 

Regards,

Bharathi

0 Kudos