[iMX6q]Capture BT.656-4 NTSC to preview, it has a screen scroll problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX6q]Capture BT.656-4 NTSC to preview, it has a screen scroll problem.

1,424 Views
xiangkunkong
Contributor II

Hi, all

We have tried two solutions at below, but both are not worked.(kernel version 3.10)

1. set active top(mxc_v4l2_capture.c) value 3, or 4, or 13

    Actully we tried 1~255...

2. Refer [5 Common issue] of i.MX6_IPU_TVIN_Application_Notes.pdf, and also tried the patch of [5.1.1 Detect NFB4EOF Error or TVIN Signal Lock Lost].

Waring log:

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x00000001        (NFB4EOF error)
imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

 

We are using tc90105fg video decoder, and known its output blanking video is unragular.

----- pre line data + EAV + blanking samples + SAV + next line data ----

the blanking samples are unragular, it's a not fixed value.

Let me know if you have any advice.

Thanks,

kong

 

0 Kudos
Reply
3 Replies

1,346 Views
xiangkunkong
Contributor II

I'm trying add vsync/hsync signal on my sabre for testing, i will back and share my result.

0 Kudos
Reply

1,410 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kong

 

IPU_INT_STAT_10 =0x00080000" points to data starvation when data that should be sent to display is not available in IPUs internal  FIFO. Most probable cause for this issue is huge load on the DDR memory bus.  One can try to set IPU prioirty higher using sect.36.4.7 GPR (IOMUXC_GPR6)

i.MX 6Dual/6Quad Applications Processor Reference Manual

 

Best regards
igor

0 Kudos
Reply

1,382 Views
xiangkunkong
Contributor II

Hi igorpadykov,

Thanks for your reply.

I tried it(0x7F007F -> 0xFF00FF), but the issue is not be fixed.

0 Kudos
Reply