iMX6ULZ SDIO version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULZ SDIO version

740 Views
jupiter_hce
Contributor III

 

Hi,

iMX6ULZ datasheet does not define the SDIO version supported, what is the iMX6ULZ SDIO version? Some WiFi modules use SDIO version 3, can it be supported?

Thank you.

Kind regards,

jupiter

 

 

Labels (1)
0 Kudos
Reply
3 Replies

725 Views
jupiter_hce
Contributor III

Hi,

Is it correct that the iMX6ULZ SDIO is a standard protocol which is able to connect to any WiFi SDIO?

If it is correct, can iMX6ULZ also connect to SDIO version 3?

Thank you very much.

Kind regards,

jh

 

 

 

0 Kudos
Reply

702 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Yes, you can it in the RM, The features of the uSDHC module include Compatible with the SDIO Card Specification version 3.0.

0 Kudos
Reply

723 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I will help confirm and then give you update

0 Kudos
Reply