iMX6ULL-evk use Murata CYW43455 module with BUILDROOT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6ULL-evk use Murata CYW43455 module with BUILDROOT

ソリューションへジャンプ
1,331件の閲覧回数
SicScar
Contributor II

Hi everybody, 

I'm trying to setup Murata Wifi Module CYW43455-1MW (I have the uSD-M2 Adapter kit) on my iMX6ULL-14x14-evk dev board, and I'm using Buildroot (version 2021-08-01) as build system. I easily found murata-cyw-fw inside the packages and set my dts for dev board imx6ull-14x14-evk-btwifi.dts . but I can't still see anything in the OS running. Except for the usdhc messages: 

[ 38.053537] mmc0: queuing unknown CIS tuple 0x80 (2 bytes)
[ 38.068525] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
[ 38.081181] mmc0: queuing unknown CIS tuple 0x80 (3 bytes)
[ 38.099778] mmc0: queuing unknown CIS tuple 0x80 (7 bytes)
[ 38.116583] mmc0: queuing unknown CIS tuple 0x80 (6 bytes)
[ 38.393765] mmc0: new ultra high speed SDR104 SDIO card at address 0001

Does anybody have exceprience with this module and how to it up with buildroot? 

Thanks so much

 

Simone

 

ラベル(3)
0 件の賞賛
返信
1 解決策
1,317件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @SicScar,

 

Unfortunate buildroot is not officially supported by NXP, you could ask on the community from Murata and see of they do, or wait for feedback that has experience on this tool.

 

Regards,

Israel.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,318件の閲覧回数
nxf63675
NXP TechSupport
NXP TechSupport

Hi @SicScar,

 

Unfortunate buildroot is not officially supported by NXP, you could ask on the community from Murata and see of they do, or wait for feedback that has experience on this tool.

 

Regards,

Israel.

0 件の賞賛
返信