iMX6ULL build with package manager

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6ULL build with package manager

2,178 次查看
michalkravcik
Contributor I

Dear all,

I just receive an i.MX6ULL evaluation kit which include  microSD card with Linux L4.1.15_2.0.1 GA.  

Linux boot well, I can use serial connection or ssh, what is very comfortable.

My problem is, I can not fid out which package manager is installed (pacman, apt-get, Yum..etc). I think there is none. Am I right?

So if I understand it correctly, I do need build new Linux sd image to have package manager. I tried to follow up a NXP/Freesacle document "Freescale Yocto Project User's Guide" . I hit a problem about board support in command $source setup-environment where is no imx6ull board.

I also tried to find something for this board on https://github.com/Freescale/meta-freescale-3rdparty but without success.

Can you please provide me how to build image for imx6ullevk or is there any official image with package manager? Am I only one how doesn't need it, or do I understand it wrong?

Thank you for your help.

I tried to find if this problem was discussed before, but I did not success.

Best regards

MK.

标签 (2)
0 项奖励
回复
1 回复

1,453 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Michal,

please take a look to the following thread Yocto with a package manager (ex: apt-get) 


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复