iMX6ULL VDD_SNVS_IN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL VDD_SNVS_IN

1,116 Views
paultran
Contributor I

hi, 

we got issue when design new iMX6ULL.

Board can boot via usb and can working but i detected issue with pin (ball pin number : p12, pin nam: VDD_SNVS_IN)

   - follow spec that pin is input power 

   - but i checked this pin may be out put and always 4.4 V. 

   - my design used PF3001 for PMU, ( 4.4v come out before 5V go through mostfet and supply for PF3001)

   - Checked and no sorted 4v4 with VDD_SNVS_IN, but so stranger 

anybody have same issue 

plz advise 

Thanks

Labels (3)
0 Kudos
Reply
1 Reply

944 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Paul Tran,

The VDD_SNVS_IN pin is indeed an input. I would recommend looking back at your design to follow up where the VDD_SNVS_IN is originated, since it’s very odd that the voltage is 4.4v. If the voltage is coming from the PF3001 I would suggest there is a problem on the PMIC configuration.

If you could provide more details maybe we can help you figure out where the problem is.

Regards,

0 Kudos
Reply