iMX6ULL-EVK: Burn u-boot, zImage, dtb file and rootfs to qspi flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6ULL-EVK: Burn u-boot, zImage, dtb file and rootfs to qspi flash

1,322 Views
chih-hunghsieh
Contributor I

Hi there,

Is there any sample vbs and ulc2 config file for mfgtool2 to burn the u-boot, zImage, device tree file and rootfs for iMX6ULL-EVK board? The default vbs and ulc2 provided by mfgtool2 only copy the u-boot to qspi flash as well as qspi header. I used the SDCard ane eMMC section in the ulc2 config as reference and tried to add my own scripts to burn the zImage, dtb and rootfs to qspi flash but failed to understand how to do partition of qspi flash.

Any tutorial available or help is appreciated.

Albert

0 Kudos
Reply
1 Reply

884 Views
igorpadykov
NXP Employee
NXP Employee

Hi CHIH-HUNG

please look at mfg tool for scm modules, it provides examples for small images

Programmers (Flash, etc.)
SCM_IMX6_M6.0.1_2.1.0_MFGTOOL
http://www.nxp.com/products/single-chip-modules/quick-start-board-for-scm-i.mx-6dq:QWKS-SCM-IMX6DQ?f...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply