Hello,
I have a custom i.MX6ULL board. I tested a set of DCP routines on a bare metal board (no OS, just asm initialization and main). Now I am trying to test these same routines after an OS has enabled the MMU. No combination of logical mmap() options seems to allow the DCP direct access to OCRAM. Is it physically possible for the DCP to operate on OCRAM when the MMU is enabled?
Thanks!
Stephen
Solved! Go to Solution.
To whom it concerns,
I found it works as long as the source buffer, destination buffer, and command are all mmap'ed such that
1) both addr and offset are the same (1st and last parameter)
2) prot = PROT_NOCACHE | PROT_READ | PROT_WRITE
3) flags = MAP_SHARED | MAP_PHYS | MAP_FIXED | MAP_NOSYNCFILE
4) fileds = NOFD
example:
#define MMAP_PROT (PROT_NOCACHE | PROT_READ | PROT_WRITE)
#define MMAP_FLAGS (MAP_SHARED | MAP_PHYS | MAP_FIXED | MAP_NOSYNCFILE)
#define MMAP_FILE_DES NOFD
srcBuf = (volatile uint32_t*) mmap((void* const)OCRAM_SRC_BUF_ADDR, OCRAM_BUF_SIZE, MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_SRC_BUF_ADDR);
dstBuf = (volatile uint32_t*) mmap((void* const)OCRAM_DST_BUF_ADDR, OCRAM_BUF_SIZE, MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_DST_BUF_ADDR);
cmd = (volatile DcpWorkPacket*) mmap((void* const)OCRAM_CMD_ADDR, sizeof(DcpWorkPacket), MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_CMD_ADDR);
This forces the mapped addresses to be the same as the physical addresses being mapped, and removes all buffering. It appears as though the DCP is incapable of IO unless the mapped addresses are the same as the physical addresses. When I remove MAP_FIXED, it fails. This may be unfortunate because not all OSs support MAP_FIXED.
To whom it concerns,
I found it works as long as the source buffer, destination buffer, and command are all mmap'ed such that
1) both addr and offset are the same (1st and last parameter)
2) prot = PROT_NOCACHE | PROT_READ | PROT_WRITE
3) flags = MAP_SHARED | MAP_PHYS | MAP_FIXED | MAP_NOSYNCFILE
4) fileds = NOFD
example:
#define MMAP_PROT (PROT_NOCACHE | PROT_READ | PROT_WRITE)
#define MMAP_FLAGS (MAP_SHARED | MAP_PHYS | MAP_FIXED | MAP_NOSYNCFILE)
#define MMAP_FILE_DES NOFD
srcBuf = (volatile uint32_t*) mmap((void* const)OCRAM_SRC_BUF_ADDR, OCRAM_BUF_SIZE, MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_SRC_BUF_ADDR);
dstBuf = (volatile uint32_t*) mmap((void* const)OCRAM_DST_BUF_ADDR, OCRAM_BUF_SIZE, MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_DST_BUF_ADDR);
cmd = (volatile DcpWorkPacket*) mmap((void* const)OCRAM_CMD_ADDR, sizeof(DcpWorkPacket), MMAP_PROT, MMAP_FLAGS, MMAP_FILE_DES, OCRAM_CMD_ADDR);
This forces the mapped addresses to be the same as the physical addresses being mapped, and removes all buffering. It appears as though the DCP is incapable of IO unless the mapped addresses are the same as the physical addresses. When I remove MAP_FIXED, it fails. This may be unfortunate because not all OSs support MAP_FIXED.