Hi,
I have been working on Rocko build from fsl-community-bsp, since last few days and able to complete the builds for our various devices which uses imx6UL and imx6Solo processors.
During testing these builds, I have encountered an issue with touch screen calibration for iMX6UL based build. So i have again tried the same build for imx6ulevk and tested on imx6UL EVK and encountered the same issue, below are the details
Machine: imx6ulevk
Image: core-image-x11
The issue I have observed on the device is, Xorg is unable to calibrate the touchscreen, I don’t know what has changed but it is unable to calibrate, below is the log
Using calibration data stored in /etc/pointercal.xinput
Invalid format 42060
unable to find device EETI eGalax Touch Screen
INFO: width=480, height=272
random: nonblocking pool is initialized
ERROR: XorgPrint Calibrator does not support the supplied --output-type
Error: unable to apply or save configuration valuesUsing calibration data stored in /etc/pointercal.xinput
Size 1024x768 not found in available modes
Invalid format 42060
unable to find device EETI eGalax Touch Screen
matchbox: Cant find a keycode for keysym 269025056
matchbox: ignoring key shortcut XF86Calendar=!$contacts
matchbox: Cant find a keycode for keysym 2809
matchbox: ignoring key shortcut telephone=!$dates
matchbox: Cant find a keycode for keysym 269025050
matchbox: ignoring key shortcut XF86Start=!matchbox-remote -desktop
INFO: width=480, height=272
ERROR: XorgPrint Calibrator does not support the supplied --output-type
Error: unable to apply or save configuration values
Does anybody faced similar issue?
Can somebody please help?
解決済! 解決策の投稿を見る。
Hi Igor,
As i said earlier, it has nothing to do with kernel version, as i have tried with 4.9.88 kernel also for imx6ulevk machine, and still seen the same issue.
I found the solution on this in one of reply from yocto community,
Actually, does not installing xf86-input-libinput helped, xinput-calibrator can not cope with that input backend
use following bbappend to achieve this
http://git.toradex.com/cgit/meta-toradex-demos.git/commit/?h=rocko-next&id=664a1926af81e49396bfe2681
18969ec2b8718cb
Thanks
Hi Alankar
from log: "unable to find device EETI eGalax Touch Screen", seems there is no
signal from touch, one can try to debug touch driver checking i2c signals with oscilloscope.
Also one can try with linux from nxp repository:
https://source.codeaurora.org/external/imx/linux-imx/tree/?h=imx_4.9.88_2.0.0_ga
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
thanks for your reply...
Actually I am not using eGalax EETI Touch screen, it should use iMX6UL's internal touchscreen controller, i am using simple resistive touch screen. Basic touch screen is working, because when during first power up when X tries to calibrate the touch screen, it is able to detect every touch but when it tries to write to /etc/pointercal.xinput it says output type is not supported, and if i look at xinput_calibrator_once.sh in /usr/bin which is called at first power up the --output-type is defined as xinput which is correct. So as it is not able to save the calibration points the touch screen doesn't work in X or in any of QT apps we are building.
I believe this is nothing do to with kernel as i am using 4.1.35 which was in morty build and where this touch calibrate is working well. i just bumped the version of all apps/rootfs to rocko so as to get all latest application versions like QT-5.9.7 etc, so i think there is something changed in X build and which is broken.
Can you please check this and let me know if anything i can try...
Thanks
Hi Alankar
I think kernel 4.1.35 may be issue as it is not among supported by nxp kernels, supported
are listed on i.MX Software|NXP
Best regards
igor
Hi Igor,
As i said earlier, it has nothing to do with kernel version, as i have tried with 4.9.88 kernel also for imx6ulevk machine, and still seen the same issue.
I found the solution on this in one of reply from yocto community,
Actually, does not installing xf86-input-libinput helped, xinput-calibrator can not cope with that input backend
use following bbappend to achieve this
http://git.toradex.com/cgit/meta-toradex-demos.git/commit/?h=rocko-next&id=664a1926af81e49396bfe2681
18969ec2b8718cb
Thanks