iMX6UL WDOG1 external signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL WDOG1 external signal

1,906 Views
philipp_blumberg
Contributor II

We are setting up the iMX internal watchdog at the moment. On our board we have routed the LCD_CLK (WDOG1_RST_B_DEB) to our reset circuitry. We have it activated in the device tree

&wdog1 { /* hw watchdog */
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_wdog1>;
   fsl,ext-reset-output;
   timeout-sec = <120>;  
          
};   
pinctrl_wdog1wdoggrp {
      fsl,pins = <
         MX6UL_PAD_LCD_CLK__WDOG1_WDOG_RST_B_DEB         0x130b1 /* WDOG_B_IMX_GPIO */
      >;
   };   

 

The pin is configured correctly (can be seen by debugger) as WDOG1_RST_B_DEB.

But, when executing echo b >/proc/sysrq-trigger for example, the board just hangs up and doesnt assert the RST_B_DEB pin low. Neither a hardware or a software reset happens. It seems like we broke the reset chain somehow by routing the RST_B_DEB to external.

Could you see any problem with that? Or do we have to use the LCD_RESET multiplex WDOG1_ANY

Labels (1)
0 Kudos
Reply
5 Replies

1,843 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philipp

one can check signal with oscilloscope and debug if necessary in driver

function  imx2_wdt_restart(), ext_reset :

imx2_wdt.c\watchdog\drivers - linux-imx - i.MX Linux kernel 

To avoid hanging it is necessary to remove shortly all power from board

as it is done on i.MX6UL EVK schematic SPF-2861 p.10 U708

Design files, including hardware schematics, Gerbers, and OrCAD files

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,843 Views
philipp_blumberg
Contributor II

Good morning Igor,

thanks for your quick reply!

As I can see from the imx2_wdt_restart() function, internal and external reset simultaneously is not possible. Understood. Our design features a reset chip, just like the EVK (STM6679Y). 

The problem is that the wdog1_rst_b_deb is not getting asserted. It is configured as such, but doesn't react. Please find the configuration  after bootup below:

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

Here is the watchdog register after sending a "echo b >/proc/sysrq-trigger" to trigger the watchdog, the system hangs up at this point because no external reset takes place. The wdog1_rst_b_deb external pin remains logical HIGH.

pastedImage_4.png

Can you please give an advice what prevents the pin from getting asserted?

Another problem is that the processor seems to loose informations about the reset cause, it displays POR on following startup, not WDOG. For sure it looses this information because of the power cycle. Do you have a solution for that?

0 Kudos
Reply

1,843 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philipp

>Can you please give an advice what prevents the pin from getting asserted?

suggest to attach jtag and test behavior setting bit with debugger and observing signal with oscilloscope.

>Another problem is that the processor seems to loose informations about the reset cause, it displays POR on following >startup, not WDOG. For sure it looses this information because of the power cycle. Do you have a solution for that?

your understanding is correct, unfortunatlely there is no solution for that.

Best regards
igor

0 Kudos
Reply

1,843 Views
philipp_blumberg
Contributor II

Hi Igor,

which bit are you exactly talking about? When setting SRS bit, it doesn't matter if wdog_rst_b_deb is configured as such or not, the pin will fall low (due to internal driver shutdown). It doesn't get asserted intentionally. WDA bit is set on watchdog triggering but the wdog_rst_b_deb bin remains high

Kind regards,

Philipp

0 Kudos
Reply

1,843 Views
igorpadykov
NXP Employee
NXP Employee

Hi Philipp

 

>which bit are you exactly talking about?
please refer to description in Refenece Manual:
pastedImage_1.jpg

 

Best regards
igor

0 Kudos
Reply