iMX6UL Reference Manual - DDR density specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6UL Reference Manual - DDR density specification

ソリューションへジャンプ
2,602件の閲覧回数
markusb
Contributor I

Hi,

in IMX6ULRM it say in 33.1.1 , that 256Mbits-8Gbits are the supported densities of DDR devices, however 6.2 specifies a density of 256Mbytes - 4Gbytes.

I suppose the first one is correct and there would be no issue using a 128MByte = 1Gbit device?

Thanks!

ラベル(1)
タグ(2)
1 解決策
2,075件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The i.MX6UL MMDC inludes the following features :

* x16 data bus width (2 bytes);

* up to 8 banks (3 bits );

* column size of 8–12 bits ;

* row size of 11–16 bits.

 

  So, minimal address size is 8 MBytes [2 ** (11+8+3+1)]

and maximal one is full 4GB.

 

128 MB is supported.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

1 返信
2,076件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   The i.MX6UL MMDC inludes the following features :

* x16 data bus width (2 bytes);

* up to 8 banks (3 bits );

* column size of 8–12 bits ;

* row size of 11–16 bits.

 

  So, minimal address size is 8 MBytes [2 ** (11+8+3+1)]

and maximal one is full 4GB.

 

128 MB is supported.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!