iMX6UL EVK MFGTools burning halt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6UL EVK MFGTools burning halt

Jump to solution
1,119 Views
shikai
Contributor I

Dear all,

     I got a new iMX6UL board(MCIMX6UL-EVK2,29013) recently, and I used MFGTools(L3.14.52_1.1.0_ga-mfg-tools) burning official images according to the doc(http://www.nxp.com/zh-Hans/files/32bit/doc/quick_start_guide/IMX6ULTRALITEQSG.pdf?fasp=1&WT_TYPE=Use... ).

     But MFGTools always halt on "Loading U-boot", and debug port no any log output in terminal(I use SecureCRT as serial terminal).

     In fact, the board packing list have a SD card (description of programmed Linux), i set boot mode from MicroSD and try use it boot board, but always no any log output from debug port.
      Dose the new board have hardware problem?
     Could you give me some suggestion?

74ec7a0c0f6a81a487f551cccf827632?fid=84105768-250528-259478039456556&time=1470978000&rt=sh&sign=FDTAER-DCb740ccc5511e5e8fedcff06b081203-hJNCjHNEkR4fRQTfBOKppRA1Dqs%3D&expires=2h&chkv=0&chkbd=0&chkpc=&dp-logid=4055520376&dp-callid=0&size=c850_u580&quality=100

Labels (1)
0 Kudos
1 Solution
884 Views
igorpadykov
NXP Employee
NXP Employee

Hi shi

there are several i.MX6UL boards, please verify board markings with below i.MX6UL EVK design schematic:

Schematics (1)

MCIMX6UL-EVK_DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 0)

http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&tab...

for programming images please use mfg tools *.vbs file, like mfgtool2-yocto-mx-evk-sdcard-sdn.vbs

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
885 Views
igorpadykov
NXP Employee
NXP Employee

Hi shi

there are several i.MX6UL boards, please verify board markings with below i.MX6UL EVK design schematic:

Schematics (1)

MCIMX6UL-EVK_DESIGNFILES

Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 0)

http://www.nxp.com/products/sensors/gyroscopes/i.mx6ultralite-evaluation-kit:MCIMX6UL-EVK?fpsp=1&tab...

for programming images please use mfg tools *.vbs file, like mfgtool2-yocto-mx-evk-sdcard-sdn.vbs

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
884 Views
shikai
Contributor I

Thank you!

I have boot the board successfully. The core-board slot is loosening and I insert it again, then everything is OK!

0 Kudos