I am trying to use the iMX6UL-EVK to boot strap a bare-metal project that will utilize the iMX6UL. As such I am trying to build u-boot for the board (using mx6ul_14x14_evk_defconfig) that will boot from qspi. Using MfgTool2, I can flash a pre-built version of u-boot into the QSPI flash, and boot from it. However, I can't seem to build a version of u-boot that will allow booting from QSPI.
Does anyone have any pointers for building a QSPI image u-boot for the imx6ul-evk?
Note: I'm currently using the git.denx.de repo
解決済! 解決策の投稿を見る。
Hi Craig
suggest to build NXP/FSL github uboot (refer to attached Release Notes Table 10)
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_3.14.52_1.1.0_ga
Board Support Packages (32)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Craig
suggest to build NXP/FSL github uboot (refer to attached Release Notes Table 10)
http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_3.14.52_1.1.0_ga
Board Support Packages (32)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------