iMX6SoloX documentation questions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SoloX documentation questions

1,831 Views
alevyzebra
Contributor I

Hi.  I have several questions regarding the LCDIF section of Freescale document IMX6SXRM.

- Table 37-2 (eLCDIF Clocks) is empty.  Clearly there are clocks required for this component, what should be in the table?

- The PANIC section in the "LCDIFx_THRES field descriptions" is empty.  I think this is what is being described in section 37.4.1.2, but the example there also contains typos.  For instance, it says "To set the panic output when 3/4s of the LFIFO is empty, set the LCDIF_THRES_PANIC value to 3/4 * 512, or 128."   I think what was meant to be written was "1/4 * 512," correct?

- Some of the LCDIF registers (e.g. LCDIFx_RLn, LCDIFx_CTRL1n, and LCDIFx_CTRL2n) indicate their addresses as "Base address + 0h offset + (4d x i) where i=0d to 3d."  Is the following correct?

   - i = 0 refers to using the "general" LCDIFx_RL register

   - i = 1 refers to using the LCDIFx_RL_SET register

   - i = 2 refers to using the LCDIFx_RL_CLR register, and

   - i = 3 refers to using the LCDIFx_RL_TOG

Thanks,

Alex

Labels (1)
Tags (1)
0 Kudos
Reply
4 Replies

1,611 Views
art
NXP Employee
NXP Employee

Q. Table 37-2 (eLCDIF Clocks) is empty. Clearly there are clocks required for this component, what should be in the table?

A. The data for this table will be added in the next document release.

Q. I think what was meant to be written was "1/4 * 512," correct?

A. Yes, this is correct.

Q. Some of the LCDIF registers (e.g. LCDIFx_RLn, LCDIFx_CTRL1n, and LCDIFx_CTRL2n) indicate their addresses as "Base address + 0h offset + (4d x i) where i=0d to 3d."  Is the following correct?

  - i = 0 refers to using the "general" LCDIFx_RL register

  - i = 1 refers to using the LCDIFx_RL_SET register

  - i = 2 refers to using the LCDIFx_RL_CLR register, and

  - i = 3 refers to using the LCDIFx_RL_TOG

A. Yes, this is correct.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,611 Views
alevyzebra
Contributor I

Additionally, I'm now looking at the timing parameters on the LCDIF.  The LCDIFx_TIMING field descriptions (section 37.6.7) reference signals that don't seem to be listed in the timing diagram in figure 37-11.  What are the DCn and CEn signals?  I'm assuming the CEn is the chip select (LCD_CS) signal, but what is the DCn signal?  My best guess is LCD_WR_RWn, but I'm not sure about that.

Thanks,

Alex

0 Kudos
Reply

1,611 Views
alevyzebra
Contributor I

Thanks for your reply, Artur.  Can you expand on what should be in table 37-2?

-Alex

0 Kudos
Reply

1,611 Views
art
NXP Employee
NXP Employee

There should be the information on the module's clocks connection within the chip.


Have a great day,
Artur

0 Kudos
Reply