iMX6SDL - OTP fuse for temperature grade?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6SDL - OTP fuse for temperature grade?

1,448 Views
timjaacks
Contributor III

Hi everyone,

on the iMX6Q there is a fuse from which you can read the temperature grade of the CPU. It can be found in the reference manual in chapter 5.2 ("Fusemap Description Table") and is located at fuse address 0x480[7:6].

For the iMX6SDL, there is no such fuse documented. I tried reading the same address, hoping that the information is there and just undocumented, but I had no luck. The according address reads 0 (= "consumer") on my device, but I know it is an "extended consumer" device.

Is there a way to find out the temperature grade of an iMX6SDL via software?

Best regards,

Tim

Labels (4)
0 Kudos
5 Replies

950 Views
timjaacks
Contributor III

Hi again,

I just saw that the speed grading is not available on the iMX6SDL, either.

There should be a way to determine temperature and speed grade at runtime, shouldn't it?

So how can I do that?

Best regards,

Tim

0 Kudos

950 Views
gusarambula
NXP TechSupport
NXP TechSupport

I’m sorry for the delay. The fuse location and bit registers are the same for S/DL as for the D/Q devices. This has already been escalated so it gets added to the next release of the S/DL Reference Manual.

Would you please confirm if the register values do match?

0 Kudos

950 Views
timjaacks
Contributor III

Thanks for your reply. Does this apply to temperature grade or speed grade or both? Are only the fuse addresses the same, or the values too?

As I said, I tried reading fuse address 0x480[7:6] (which is temperature grade on the iMX6DQ) on an iMX6SDL. I expected to read a "1" (= "Extended Commercial", that is my device), but I got a "0" (= "Commercial"). Thus, I assume that 0x480[7:6] does not report the temperature grade on the iMX6SDL, or the interpretation of the bits is different.

0 Kudos

950 Views
gusarambula
NXP TechSupport
NXP TechSupport

Would you please share the complete Part Number of your i.MX6 device?

0 Kudos

950 Views
timjaacks
Contributor III

This is the part number of my device: MCIMX6S5EVM10AB

I am using Linux kernel 3.0.35 and tried:

cat /sys/fsl_otp/HW_OCOTP_MEM0

which returns 0x0.

On an i.MX6DQ Extended Consumer device (MCIMX6D5EYM10AC) I am reading a correct value 0x40 here.

0 Kudos