Hi All
I am trying to operate the PCIe bus board on the IMX6QSABRESD board by referring to i.MX Yocto Project User's Guide (Rev. L5.4.70_2.3.0 — 31 December 2020). However, it does not detect the PCI bus. If it is an old environment, it is detected as (* 2). I thought that the Kernel Config setting was insufficient, so I tried to modify the setting with "bitbake virtual / kernel -c menuconfig", but it was not detected. Please tell me the settings.
An excerpt of the settings at the time of kernel build is posted in (* 3).
Attach the config file.
Best Regards
Hiroaki Okoshi
Kernel 5.4.70 Log(*1)
root@imx6qsabresd:~# uname -a
Linux imx6qsabresd 5.4.70-2.3.0+g4f2631b022d8 #1 SMP PREEMPT Wed Jan 27 09:32:30 UTC 2021 armv7l GNU/Linux
root@imx6qsabresd:~# lspci
root@imx6qsabresd:~# lspci --version
lspci version 3.6.2
root@imx6qsabresd:~# dmesg | grep PCI
[ 0.185030] PCI: CLS 0 bytes, default 64
[ 1.715928] ehci-pci: EHCI PCI platform driver
Kernel 4.14.98 Log(*2)
root@imx6qsabresd:~# uname -a
Linux imx6qsabresd 4.14.98-imx_4.14.98_2.0.0_ga+g5d6cbeafb80c #1 SMP PREEMPT Thu Jan 7 23:18:46 UTC 2021 armv7l GNU/Linux
root@imx6qsabresd:~# lspci
00:00.0 PCI bridge: Synopsys, Inc. Device abcd (rev 01)
01:00.0 Network controller: Broadcom Limited Device 43ef (rev 05)
root@imx6qsabresd:~# lspci --version
lspci version 3.5.6
Build Setting
user@RZ3900:~/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/5.4-r0$ grep IMX defconfig
CONFIG_SOC_IMX50=y
CONFIG_SOC_IMX51=y
CONFIG_SOC_IMX53=y
CONFIG_SOC_IMX6Q=y
CONFIG_SOC_IMX6SL=y
CONFIG_SOC_IMX6SLL=y
CONFIG_SOC_IMX6SX=y
CONFIG_SOC_IMX6UL=y
CONFIG_SOC_IMX7D=y
CONFIG_SOC_IMX7ULP=y
CONFIG_ARM_IMX6Q_CPUFREQ=y
CONFIG_ARM_IMX_CPUFREQ_DT=y
CONFIG_ARM_IMX7ULP_CPUFREQ=y
CONFIG_PCI_IMX6_HOST=y
CONFIG_PCI_IMX6_EP=y
CONFIG_IMX_WEIM=y
CONFIG_AHCI_IMX=y
CONFIG_PATA_IMX=y
CONFIG_KEYBOARD_IMX=y
CONFIG_TOUCHSCREEN_IMX6UL_TSC=y
CONFIG_SENSOR_IMX_RPMSG=y
CONFIG_SERIAL_IMX=y
CONFIG_SERIAL_IMX_CONSOLE=y
CONFIG_I2C_IMX=y
CONFIG_I2C_IMX_LPI2C=y
CONFIG_SPI_IMX=y
CONFIG_GPIO_IMX_RPMSG=y
CONFIG_IMX_THERMAL=y
CONFIG_IMX2_WDT=y
CONFIG_IMX7ULP_WDT=y
CONFIG_VIDEO_IMX_PXP=y
CONFIG_SND_IMX_SOC=y
CONFIG_SND_SOC_IMX_WM8960=y
CONFIG_SND_SOC_IMX_SII902X=y
CONFIG_SND_SOC_IMX_WM8958=y
CONFIG_SND_SOC_IMX_CS42888=y
CONFIG_SND_SOC_IMX_WM8962=y
CONFIG_SND_SOC_IMX_RPMSG=y
CONFIG_SND_SOC_IMX_ES8328=y
CONFIG_SND_SOC_IMX_SGTL5000=y
CONFIG_SND_SOC_IMX_MQS=y
CONFIG_SND_SOC_IMX_SPDIF=y
CONFIG_SND_SOC_IMX_MC13783=y
CONFIG_SND_SOC_IMX_SI476X=y
CONFIG_SND_SOC_IMX_HDMI=y
CONFIG_MMC_SDHCI_ESDHC_IMX=y
CONFIG_RTC_DRV_IMX_RPMSG=y
CONFIG_IMX_SDMA=y
CONFIG_IMX_MBOX=y
CONFIG_IMX_REMOTEPROC=y
CONFIG_IMX7D_ADC=y
CONFIG_PWM_IMX27=y
CONFIG_PWM_IMX_TPM=y
CONFIG_NVMEM_IMX_OCOTP=y
user@RZ3900:~/tmp/work/imx6qsabresd-poky-linux-gnueabi/linux-imx/5.4-r0$ grep PCI defconfig
CONFIG_PCI=y
CONFIG_PCI_MSI=y
CONFIG_PCI_IMX6_HOST=y
CONFIG_PCI_IMX6_EP=y
CONFIG_PCI_ENDPOINT=y
CONFIG_PCI_ENDPOINT_CONFIGFS=y
CONFIG_PCI_EPF_TEST=y
CONFIG_PCI_ENDPOINT_TEST=y
In the original environment, I replaced the dtb file and it worked. Is it the only way to copy it manually?
Thanks
Hi HiroakiOkoshi
one can try with Demo Image : i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualLite, i.MX 6SoloX Boards
also recommended to test with several pcie cards.
Best regards
igor
I was able to do it, but I failed to POST many times, so I lost the desire to POST.