iMX6Q usdhc4 and gpmi muxing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q usdhc4 and gpmi muxing

1,740 Views
harshakumar
Contributor II

Can some one tell how to mux gpmi NAND and usdhc4 pins in imx6 Quad core processor.NAND_RE uses SD4_CMD and NAND_WE uses SD4_CLK PadNets.No other mux option is given.I am using all 4 usdhc for SDIO interfaces and NAND flash for memory.If not able to mux please suggest some SDIO expander chip compatible with imx6Q processor.Please Help

0 Kudos
Reply
3 Replies

1,630 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harsha

for sd one can try spi option with probably some external circuitry or OneNand (weim interface)

or external controllers like, CYWB0124

http://www.mouser.com/ds/2/100/001-07978_CYWB0124AB_CYWB0125AB_WEST_BRIDGE_ANTIOC-369138.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,630 Views
harshakumar
Contributor II

Hi igor

Thanks for suggestion, I am planning to use SDIO port expander TXS02612RTWR which supports two SDXC cards.

But problem is handling card detection interrupt since one card detection pin available in processor side.Can I have any suggestion 

Regards,

Harsha 

0 Kudos
Reply

1,630 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harsha

one can use GPIO for card detection, please refer to sect.32.3.3 Devicetree Binding

attached Linux Manual.

Best regards
igor

0 Kudos
Reply