I am Using iMX6Q - sabresd cusomised board to boot android and linux , the panel type model is KD101N70-40NV-A002, 10.1", TFT LCD , IC:0TD7107B-C/OTD9800A-C8 driver . It works fine in android but fails to get display when I boot in Linux. We set the resolution as 1280x800 in dtb file .. we are to boot the linux upto command mode .. Unable to get the graphical display in linux ( debian based OS ). Is the panel K&D- WXGA has support in linux or not..
Hi Ganesh
this depends on used bsp, nxp linux documentation describes supported
panels in Release Notes, found in linux doc package
https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS
other vendors may support more panels, for example on below link
Configuring i.MX6 boards for different screens - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------