iMX6Q sabre uboot file for microSD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q sabre uboot file for microSD card

1,006 次查看
dibing
Contributor I

Hi

i have designed a vehicle infotainment system using iMX6Q processor in sabre platform. 

In my design, i updated the bootable SD card with microSD card.

When I am loading the uboot file, it shows that "no device found"because of the pin change of SDcard Card detection pin.

In microSD card, CD and Data3 are multiplexed. 

Please help me to boot the system without the Card Detection function...

0 项奖励
回复
1 回复

901 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Dibin

please look at board_mmc_getcd() in uboot/board/freescale/mx6sabresd/mx6sabresd.c

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复