iMX6Q sabre uboot file for microSD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q sabre uboot file for microSD card

1,016 Views
dibing
Contributor I

Hi

i have designed a vehicle infotainment system using iMX6Q processor in sabre platform. 

In my design, i updated the bootable SD card with microSD card.

When I am loading the uboot file, it shows that "no device found"because of the pin change of SDcard Card detection pin.

In microSD card, CD and Data3 are multiplexed. 

Please help me to boot the system without the Card Detection function...

0 Kudos
Reply
1 Reply

911 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dibin

please look at board_mmc_getcd() in uboot/board/freescale/mx6sabresd/mx6sabresd.c

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply