iMX6Q not detecting in serial download mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q not detecting in serial download mode

1,170 Views
riteshpatel
Contributor II

Hi, 

I have two boards which are not detecting in USB serial download mode to flash U-boot and Kernal image.

All power to the processor is working fine. Reset sequence is proper and Reset logic state is High after power up.

The Boot mode selection pin settings are proper with proper logic level.

Is there any way to debug using JTAG interface? We have JTAG interface on our board. If yes, can you suggest the connection and required JTAG debugger tool?

Any other suggestions would be greatly appreciated.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

970 Views
joanxie
NXP TechSupport
NXP TechSupport

yes you can use Jtag, more detailed information, pls refer to the link as below:

https://community.nxp.com/message/953055?commentID=953055#comment-953055

0 Kudos
Reply