iMX6Q VPU performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q VPU performance

716 Views
kristofferglemb
Contributor III

What settings would give lower memory load?

Anyway I think someone at Freescale should be able to answer if it is possible to encode 1920x1080 @ 30 fps with memory running at 396 MHz or if it is some other issue we are facing.

0 Kudos
Reply
1 Reply

593 Views
Yuri
NXP Employee
NXP Employee

Hello,

  You may try the following :

1.

  Make sure below QoS settings are done in u-boot DCD table:

 /* enable AXI cache for VDOA/VPU/IPU */

 DATA 4 0x020e0010 0xF00000CF

 /* set IPU AXI-id0 Qos=0xf(bypass) AXI-id1 Qos=0x7 */

DATA 4 0x020e0018 0x007F007F

DATA 4 0x020e001c 0x007F007F

 

2.
  Force CPU to run at maximal frequency 

$ echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

https://community.nxp.com/message/598408  

0 Kudos
Reply