Hi all,
The mfw_isink is not working on Ubuntu as well as OE Yocto. It's only working on LTIB!
Is there any intention for fix this important element?
Command line and output:
linaro@linaro-ubuntu-desktop:~/Videos$ gst-launch playbin2 uri=file:/home/linaro/Videos/bunny.mp4 video-sink=mfw_isink
set color key
MFW_GST_ISINK_PLUGIN 3.0.5 build on Dec 14 2012 14:02:16.
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
Aiur: 3.0.5
Core: MPEG4PARSER_06.04.25 build on Dec 10 2012 16:29:48
mime: video/quicktime; audio/x-m4a; application/x-3gp
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///home/linaro/Videos/bunny.mp4
Idx File:
/home/linaro/.aiur/.home.linaro.Videos.bunny.mp4.aidx
Seekable : Yes
Size(byte): 5103296
Movie Info:
Seekable : Yes
Live : No
Duration : 0:00:33.041668000
ReadMode : File
Track : 2
Track 00 [video_000000] Enabled
Duration: 0:00:32.480000000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, width=(int)720, height=(int)406, framerate=(
fraction)25/1, codec_data=(buffer)000000016742c01e9a7381686bf3602200000300020000
0300651e2c5cf00000000168ce32c8
[INFO] Product Info: i.MX6Q/D/S
vpudec versions :smileyhappy:
plugin: 3.0.5
wrapper: 1.0.28(VPUWRAPPER_ARM_LINUX Build on Dec 14 2012 12:23:57)
vpulib: 5.4.10
firmware: 2.1.8.34588
Track 01 [audio_000000] Enabled
Duration: 0:00:33.041668000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)8
3680, framed=(boolean)true, stream-format=(string)raw, codec_data=(buffer)121056
e500
Cannot connect to server socket err = No such file or directory
Cannot connect to server socket
jack server is not running or cannot be started
/usr/bin/pulseaudio: error while loading shared libraries: libpulsecommon-1.0.so: cannot open shared object file: No such file or directory
Beep: 3.0.5
Core: AAC-Plus decoder Wrapper build on Nov 29 2012 14:46:30
mime: audio/mpeg, mpegversion=(int){2,4}
file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacplusd_wrap_arm12_elinux.so.3
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.07.00 build on Jul 17 2012 17:47:46.
BLN_MAD-MMCODECS_AACPD_ARM_03.07.00_ARM11 build on Jul 17 2012 17:58:59.
[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0
hwbuf allocator zone(450560) created
can not create threadmfw_gst_isink_setcaps:1489
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
VS0 created. in fmt[NV12] win(0,0-720,400:720x400) out win(0,0-1280,720:1280x720)
set deinterlace mode 0
New clock: GstAudioSinkClock
hwbuf allocator zone(614400) created
hwbuf allocator zone(614400) destroied.
hwbuf allocator zone(614400) created
hwbuf allocator zone(614400) destroied.
hwbuf allocator zone(614400) created
hwbuf allocator zone(614400) destroied.
已解决! 转到解答。
Tarek, I just tried this on an i.MX6SDP board with the following command-line.
export VSALPHA=1
gst-launch playbin2 uri=file:///
home/linaro/Videos/sample.mp4 video-sink="mfw_isink device=/dev/video16"
I get the same error:
can not create threadmfw_gst_isink_setcaps:1489
but it still plays.
BR
Mark
Tarek, I just tried this on an i.MX6SDP board with the following command-line.
export VSALPHA=1
gst-launch playbin2 uri=file:///
home/linaro/Videos/sample.mp4 video-sink="mfw_isink device=/dev/video16"
I get the same error:
can not create threadmfw_gst_isink_setcaps:1489
but it still plays.
BR
Mark
Hi Mark,
Thank you very much. When I used the same command line you provided it's working fine. I was missing the export VSALPHA=1
Now I would like to understand which fbdev it's drawing to and which fbdev i should draw my GUI to?
The video is played in the FG plane while I need it be in the BG plane.
That's going to help me a lot.
BR,
Tarek
Hi Tarek
Have a look at the vssconfig file in /usr/share
The default setting is fb_num =1 which is fb1. If you change this to fb0 it has the interesting effect making the Ubuntu desktop disappear.
Mark
You have already reported in
https://bugzilla.yoctoproject.org/show_bug.cgi?id=3781
Send a email to the meta-fsl list for an update.
Leo
Hi Leonardo,
Yes, I'm still waiting for a solution on Yocto but this post is for Ubuntu.
Unless it's going to be fixed automatically for both.
Please let me know so I can close this one.
Thanks,
Tarek