Hello all,
SITUATION: We are developing USB device on custom iMX6Q Linux based board (linux-4.1-fslc). Currently we want to use our board as a mass storage device. Loading g_mass_storage module works and host PC is able to access exported secondary disk.
PROBLEM: The problem is that before loading g_mass_storage module we need to unmount disk to be later used as an exported file. We want to do this automatically without requiring user input/interaction.
CURRENT PROGRESS: We have tried to use debug options for UDC controller (CHIPIDEA_DEBUG=y) which displays resume/suspend events on dmesg when plug/unplugg-ing USB cable.
Output:
[pluging-in USB cable]
[root@imx6 ~]# dmesg
[ 4106.637189] imx_usb 2184000.usb: at imx_controller_resume
[ 4106.637208] wakeup int at ci_hdrc.0
[ 4106.637225] ci_hdrc ci_hdrc.0: at ci_controller_resume
[ 4109.004585] ci_hdrc ci_hdrc.0: at ci_runtime_suspend
[ 4109.004635] imx_usb 2184000.usb: at imx_controller_suspend
[unpluging USB cable]
[ 4111.910737] imx_usb 2184000.usb: at imx_controller_resume
[ 4111.910753] wakeup int at ci_hdrc.0
[ 4111.910770] ci_hdrc ci_hdrc.0: at ci_controller_resume
[ 4114.004587] ci_hdrc ci_hdrc.0: at ci_runtime_suspend
[ 4114.004632] imx_usb 2184000.usb: at imx_controller_suspend
[root@imx6 ~]#Also you can see /proc/interrupts increments on such events:
[root@imx6 ~]# cat /proc/interrupts | grep -i 2184000.usb
278: 18 0 0 0 GPC 43 Edge 2184000.usb
[unplugging USB cable]
[root@imx6 ~]# cat /proc/interrupts | grep -i 2184000.usb
278: 21 0 0 0 GPC 43 Edge 2184000.usb
[root@imx6 ~]#But you can actually suppress such events by writing -1 to autosuspend_delay_ms:
echo -1 > /sys/bus/platform/drivers/ci_hdrc/ci_hdrc.0/power/autosuspend_delay_msQUESTION: How can we detect host PC connect/disconnect events? How to export those events to userspace?
We are open for any possible solution whether it is kernelspace (patching kernel) or userspace (daemon)...
Thanks,
regards!
Primoz
Although it's been some time since you posted this question, from userspace you can read.
/sys/bus/platform/drivers/ci_hdrc/ci_hdrc.0/power/runtime_status
or the same from here:
/sys/devices/soc0/soc/2100000.aips-bus/2184000.usb/power/runtime_status
If USB cable is plugged/unplugged you'll read active/suspended.
Regards
Hi Primoz,
You could take a look at USB erratas of i.MX6, which are related to suspend/resume issues:
http://www.nxp.com/files/32bit/doc/errata/IMX6DQCE.pdf
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
here is a quick update on how USB device port is actually wired to SoC:
As you can see I have just D+ and D- routed to my SoC, while +5V (from host) is basically just wired to capacitor and then to the GND.
VBUS sensing/detection over extcon framework is probably not possible with such configuration...?
Any other ideas?
Primoz