iMX6Q USB client full-speed eye-diagram issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6Q USB client full-speed eye-diagram issue

913 Views
Tony1z
Contributor I

Hi Sir,

       We designed our board with iMX6Q and measured USB client full-speed eye-diagram.

       The USB signal voltage level in full-speed cannot reach 3.3V. USB traces impedance is 90 ohm differential controlled.

       We tried to increase amplitude with setting register USBPHY1.TX.D_CAL=0x0 by memtool.

       The amplitude of full-speed USB signal increase a little but still cannot reach 3.3V. It only has around 2.6V amplitude. (Refer to attached bmp file)

       Any other software suggestion ?

Labels (1)
0 Kudos
1 Reply

712 Views
igorpadykov
NXP Employee
NXP Employee

Hi Tony1z

available software configuration is given in AN 4589

Configuring USB on i.MX 6 Series Processors sect.4.3.3 Operational settings

http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf

If this does not help, it is necessary to look at hardware methods for improving

signal quality.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos