Hi, I am new to "Boundary Devices". I have iMX6 Sabre Lite DVK and I wish to set it up. So I started with U-boot image (u-boot.nitrogen6q) flash to NOR for auto boot (using sb_loader) from NOR, not from SD. After flash set fuses on U-Boot like...
U-Boot > fuse prog 0 5 18000030
U-Boot > fuse prog 0 6 10
U-Boot > fuse prog 4 3 19
U-Boot > fuse prog 4 2 b803a949
After, prepared one SD with Ubuntu Xenial Image "20170619-nitrogen-4.1.15_2.0.0_ga-xenial-en_US-mate_armhf.img". Then when its boot and display the process on terminal. I can see the login prompt like:
xenial-dev login:
Unable to write login name, nothing is happening. Please suggest. Thanks
Thank you @gary_bisson @igorpadykov for your kind and valuable suggestions. I resolved it and enter to the board. Thanks.
Hi,
As the release post explains, the credentials are:
login: ubuntu
pwd: Boundary
Regards,
Gary
Hello @gary_bisson; thanks for your reply. But the issue is i am unable to type anything infront of login prompt. I don't understand why it get stucked after login prompt. Please suggest.
Hi,
Can you type something in the U-Boot prompt?
Usually this happens when your serial connection is not setup properly:
https://boundarydevices.com/just-getting-started/
Regards,
Gary
Hi i_ashok_s
one can look at boundary devices ubuntu tutorials
https://boundarydevices.com/wiki/bd-sl-imx6/
Best regards
igor
Thank you @igorpadykov but i followed the same tutorial but failed to login.
Please suggest. Thanks.
this software was developed and supported by boundary devices,
suggest to apply to support :
https://boundarydevices.com/software/
Best regards
igor
Thanks @igorpadykov But when I tried to send a email to support, I got this.
The following recipient(s) cannot be reached: 'Support@boundarydevices.com.'
there is another contact on link
Best regards
igor
Thanks @igorpadykov But Isn't it for Nitogen8M platform boards. Since i am using iMX6 SABRELITE, would it support that?