[iMX6Q Sabre Lite Unable to Login Ubuntu-Xenial]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[iMX6Q Sabre Lite Unable to Login Ubuntu-Xenial]

2,095 Views
i_ashok_s
Contributor I

Hi, I am new to "Boundary Devices". I have iMX6 Sabre Lite DVK and I wish to set it up. So I started with U-boot image (u-boot.nitrogen6q) flash to NOR for auto boot (using sb_loader) from NOR, not from SD. After flash set fuses on U-Boot like...

U-Boot > fuse prog 0 5 18000030

U-Boot > fuse prog 0 6 10

U-Boot > fuse prog 4 3 19

U-Boot > fuse prog 4 2 b803a949

After, prepared one SD with Ubuntu Xenial Image "20170619-nitrogen-4.1.15_2.0.0_ga-xenial-en_US-mate_armhf.img". Then when its boot and display the process on terminal. I can see the login prompt like:
xenial-dev login: 

Unable to write login name, nothing is happening. Please suggest. Thanks

Labels (1)
0 Kudos
10 Replies

1,921 Views
i_ashok_s
Contributor I

Thank you @gary_bisson @igorpadykov  for your kind and valuable suggestions. I resolved it and enter to the board. Thanks.

0 Kudos

2,043 Views
gary_bisson
Senior Contributor III

Hi,

As the release post explains, the credentials are:

login: ubuntu

pwd: Boundary

Regards,

Gary

0 Kudos

2,032 Views
i_ashok_s
Contributor I

Hello @gary_bisson; thanks for your reply. But the issue is i am unable to type anything infront of login prompt. I don't understand why it get stucked after login prompt. Please suggest.

0 Kudos

2,012 Views
gary_bisson
Senior Contributor III

Hi,

Can you type something in the U-Boot prompt?

Usually this happens when your serial connection is not setup properly:

https://boundarydevices.com/just-getting-started/

Regards,

Gary

0 Kudos

2,090 Views
igorpadykov
NXP Employee
NXP Employee

Hi i_ashok_s

 

one can look at boundary devices ubuntu tutorials

https://boundarydevices.com/wiki/bd-sl-imx6/

 

Best regards
igor

0 Kudos

2,082 Views
i_ashok_s
Contributor I

Thank you @igorpadykov but i followed the same tutorial but failed to login.

Please suggest. Thanks.

0 Kudos

2,073 Views
igorpadykov
NXP Employee
NXP Employee

this software was developed and supported by boundary devices,

suggest to apply to support :

https://boundarydevices.com/software/

 

Best regards
igor

0 Kudos

2,058 Views
i_ashok_s
Contributor I

Thanks @igorpadykov But when I tried to send a email to support, I got this.

The following recipient(s) cannot be reached:  'Support@boundarydevices.com.'

0 Kudos

2,054 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos

2,027 Views
i_ashok_s
Contributor I

Thanks @igorpadykov But Isn't it for Nitogen8M platform boards. Since i am using iMX6 SABRELITE, would it support that?

0 Kudos