iMX6Q SDRAM Size Change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6Q SDRAM Size Change

897 次查看
DaengCheong
Contributor II

I am using MT41K128M16JT memory from Micron. However, RAM capacity is not allocated from 1GB to 2GB. Please consider it.

I wrote it based on the wandboard.

U-boot 2015-04 

#include <asm/arch/clock.h>
#include <asm/arch/imx-regs.h>
#include <asm/arch/iomux.h>
#include <asm/arch/mx6-pins.h>
#include <asm/errno.h>
#include <asm/gpio.h>
#include <asm/imx-common/iomux-v3.h>
#include <asm/imx-common/video.h>
#include <mmc.h>
#include <fsl_esdhc.h>
#include <asm/arch/crm_regs.h>
#include <asm/io.h>
#include <asm/arch/sys_proto.h>

#include <common.h>

#include <spl.h>

#ifdef CONFIG_APX_WATCHDOG
#include <watchdog.h>
#endif

DECLARE_GLOBAL_DATA_PTR;

#if defined(CONFIG_SPL_BUILD)
#include <asm/arch/mx6-ddr.h>

/*
* Driving strength:
* 0x30 == 40 Ohm
* 0x28 == 48 Ohm
*/
#define IMX6DQ_DRIVE_STRENGTH 0x30

/* configure MX6Q/DUAL mmdc DDR io registers */
static struct mx6dq_iomux_ddr_regs mx6dq_ddr_ioregs = {
.dram_sdclk_0 = 0x00020030,
.dram_sdclk_1 = 0x00020030,
.dram_cas = 0x00020030,
.dram_ras = 0x00020030,
.dram_reset = 0x00020030,
.dram_sdcke0 = 0x00003000,
.dram_sdcke1 = 0x00003000,
.dram_sdba2 = 0x00000000,
.dram_sdodt0 = 0x00003030,
.dram_sdodt1 = 0x00003030,
.dram_sdqs0 = 0x00000030,
.dram_sdqs1 = 0x00000030,
.dram_sdqs2 = 0x00000030,
.dram_sdqs3 = 0x00000030,
.dram_sdqs4 = 0x00000030,
.dram_sdqs5 = 0x00000030,
.dram_sdqs6 = 0x00000030,
.dram_sdqs7 = 0x00000030,
.dram_dqm0 = 0x00020030,
.dram_dqm1 = 0x00020030,
.dram_dqm2 = 0x00020030,
.dram_dqm3 = 0x00020030,
.dram_dqm4 = 0x00020030,
.dram_dqm5 = 0x00020030,
.dram_dqm6 = 0x00020030,
.dram_dqm7 = 0x00020030,
};

/* configure MX6Q/DUAL mmdc GRP io registers */
static struct mx6dq_iomux_grp_regs mx6dq_grp_ioregs = {
.grp_ddr_type = 0x000C0000,
.grp_ddrmode_ctl = 0x00020000,
.grp_ddrpke = 0x00000000,
.grp_addds = 0x00000030,
.grp_ctlds = 0x00000030,
.grp_ddrmode = 0x00020000,
.grp_b0ds = 0x00000030,
.grp_b1ds = 0x00000030,
.grp_b2ds = 0x00000030,
.grp_b3ds = 0x00000030,
.grp_b4ds = 0x00000030,
.grp_b5ds = 0x00000030,
.grp_b6ds = 0x00000030,
.grp_b7ds = 0x00000030,
};


/* MT41K128M16JT-125 */
static struct mx6_ddr3_cfg mt41k128m16jt_125 = {
.mem_speed = 1600,
.density = 2,
.width = 16,
.banks = 8,
.rowaddr = 14,
.coladdr = 10,
.pagesz = 2,
.trcd = 1375,
.trcmin = 4875,
.trasmin = 3500,
.SRT = 0,
};

static struct mx6_mmdc_calibration mx6q_2g_mmdc_calib = {
.p0_mpwldectrl0 = 0x001F001F,
.p0_mpwldectrl1 = 0x001F001F,
.p1_mpwldectrl0 = 0x00440044,
.p1_mpwldectrl1 = 0x00440044,
.p0_mpdgctrl0 = 0x434B0350,
.p0_mpdgctrl1 = 0x034C0359,
.p1_mpdgctrl0 = 0x434B0350,
.p1_mpdgctrl1 = 0x03650348,
.p0_mprddlctl = 0x4436383B,
.p1_mprddlctl = 0x39393341,
.p0_mpwrdlctl = 0x35373933,
.p1_mpwrdlctl = 0x48254A36,
};

/* DDR 64bit 2GB */
static struct mx6_ddr_sysinfo mem_qdl = {
.dsize = 2,
.cs_density = 32,
.ncs = 1,
.cs1_mirror = 0,
.rtt_wr = 2, /* RZQ = 120 */
.rtt_nom = 2, /* RZQ = 120 */
.walat = 1,
.ralat = 5,
.mif3_mode = 3,
.bi_on = 1,
.sde_to_rst = 0x10,
.rst_to_cke = 0x23,
};

static void spl_dram_init(void)
{
mx6dq_dram_iocfg(64, &mx6dq_ddr_ioregs, &mx6dq_grp_ioregs);
mx6_dram_cfg(&mem_qdl, &mx6q_2g_mmdc_calib, &mt41k128m16jt_125);
udelay(100);
}

标签 (1)
0 项奖励
回复
0 回复数