Hi,
In our custom iMX6q board we are using LPDDR2 MT42L128M64D2LL-25 RAM. The MMDC channels are configured by using the Mx6DQSDL LPDDR2 Script Aid V0.04-new.xlsx script. Please refer the attached script.
The DDR configuration is done thru DCD settings in our custom boot loader.
Now i load the DDR calibration tool (i.MX6/7 DDR Stress Test Tool V2.20) from my boot loader. The DDR calibartion binary image is started.
But while starting DDR calibaration it stops at Test Channel 0.
Also i attached the DDR stree test binary image log.
Let me know if i miss anything.
Thanks in advance.
Regards,
Selvakumar V
Original Attachment has been moved to: DDR_StressTest.log.zip
Hello,
have You tried (to use) and change the init script (RealView.inc)
as recommended in the following thread https://community.freescale.com/docs/DOC-105652#comment-31888
Also, please look at the following : DDR stress tester V2.00 problem with i.MX6 solo lite interfacing with DDR3
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------