Hello,
I'm using a MIPI-DSI panel and trying to config the timing modifying the file: mxcfb_hx8369_wvga.c.
I can communicate with the panel controller in LP mode. I can get the status and setup other registers. However, the display don't show anything.
According with the panel controller, the clock period in HS mode must be greater than 4 ns however in the scope is 3sns. So, I think this could be the problem. To change the HS clock period I use the variable "max_phy_clk", however, the LP clock is also changed and I cannot setup the panel register (in LP mode).
Can I change the HS and LP clock independently?
Thanks for any suggestions,
JC
Solved! Go to Solution.
I found the MIPI-DSI specifications and figure out the modification. I adjust the register: TX_ESC_CLK_DIVIDSION and now the clock in command mode is OK (independently of the video mode).
Hello community,
I attached a image showing two test case using a MIPI-DSI display with an iMX6Q.
I would like to change the mipi-dsi driver to adjust a different clock for command mode and another for video mode. However, that's is impossible without the data sheet that explain the DSI module. I didn't find that.
If somebody have other ideas, don't hesitate to share it.
Thanks
JC
I found the MIPI-DSI specifications and figure out the modification. I adjust the register: TX_ESC_CLK_DIVIDSION and now the clock in command mode is OK (independently of the video mode).
Hi,
Can anyone suggest me, the procedure for MIPI DSI Host Configuration,
I have a scenario, MIPI DSI Host controller can support/operate at 1Gbps/lane(1000Mbps/lane) & getting the clock of 500MHz on CLKP & CLKN (Bit clock) , Had MIPI DSI LCD HX8260 Can operate at (480Mbps/lane),
so we need to change/down grade clock at MIPI DSI Host?
Based on the table:
/* configure data for DPHY PLL 27M reference clk out */ static const struct _mipi_dsi_phy_pll_clk mipi_dsi_phy_pll_clk_table[] = { {1000, 0x74}, /* 950-1000MHz */ {950, 0x54}, /* 900-950Mhz */ {900, 0x34}, /* 850-900Mhz */ {850, 0x14}, /* 800-850MHz */ {800, 0x32}, /* 750-800MHz */ {750, 0x12}, /* 700-750Mhz */ {700, 0x30}, /* 650-700Mhz */ {650, 0x10}, /* 600-650MHz */ {600, 0x2e}, /* 550-600MHz */ {550, 0x0e}, /* 500-550Mhz */ {500, 0x2c}, /* 450-500Mhz */ {450, 0x0c}, /* 400-450MHz */ {400, 0x4a}, /* 360-400MHz */ {360, 0x2a}, /* 330-360Mhz */ {330, 0x48}, /* 300-330Mhz */ {300, 0x28}, /* 270-300MHz */ {270, 0x08}, /* 250-270MHz */ {250, 0x46}, /* 240-250Mhz */ {240, 0x26}, /* 210-240Mhz */ {210, 0x06}, /* 200-210MHz */ {200, 0x44}, /* 180-200MHz */ {180, 0x24}, /* 160-180MHz */ {160, 0x04}, /* 150-160MHz */ };
| Horizontal Parameters | |||
| Parameter | Symbol | Value | Units |
| Horizontal Sync/ Horizontal Low pulse width | HS | 24 | DCK |
| Horizontal Back porch | HBP | 24 | DCK |
| Horizontal Front Porch | HFP | 72 | DCK |
| Horizontal Active Area | HDISP | 800 | DCK |
| Total Clocks per line | 920 | Clocks/line | |
| Vertical Parameters | |||
| Parameter | Symbol | Value | Units |
| Vertical Sync/ Vertical Low pulse width | VS | 2 | Line(s) |
| Vertical Back porch | VBP | 10 | Line(s) |
| Vertical Front Porch | VFP | 12 | Line(s) |
| Vertical Active Area | VDISP | 1280 | Line(s) |
| Lines per frame | 1304 | Line(s)/frame | |
Q) We need to configure the DSI Pixel clock , Polarity on MIPI DSI Host side? (correct me if I am wrong)
Q) we have 3 type of video modes [Video with Burst, Non Burst with Pulses, Non burst with Event sync] in MIPI DSI Host.
Q) How do we configure for Non burst with Event Sync in i.MX6, MIPI DSI Host.
Please anyone review and and let me know the procedure is correct or not , Please provide your inputs,