iMX6Dual : About the DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE for DDR3L

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6Dual : About the DDR_SEL setting of IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE for DDR3L

跳至解决方案
632 次查看
koichisakagami
Contributor II

Dear community,

We hope to know the DDR_SEL setting of the IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE register.
We know that the register should be set according to description in RM:


  10 : LPDDR2
  11 : DDR3

[Question]


When we use the DDR3L ,
Which setting should we use ,"10" or "00"
on IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE : DDR_SEL ?

Best Regards,
Koichi Sakagami

0 项奖励
回复
1 解答
522 次查看
Yuri
NXP Employee
NXP Employee

Please use DDR_SEL = DDR3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
523 次查看
Yuri
NXP Employee
NXP Employee

Please use DDR_SEL = DDR3.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复