iMX6DP/QP and eMMC HS200 mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6DP/QP and eMMC HS200 mode

ソリューションへジャンプ
1,802件の閲覧回数
JohnDoe1z
Contributor III

Hello,

the iMX6 DualPlus reference manual states that the uSDHC supports the MMC HS200 mode (section 68.1.2.1). However, the uSDHC driver coming with linux 4.9.11 does not advertise the HS200 mode for the DP/QP variants.

Is the HS200 mode supported by the iMX6 DP/QP and if so, why is the driver not reflecting that?

BR

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,512件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JohnDoe1z

it does not support HS200 mode and latest rev.1 Reference Manual (2017)

has not reference to HS200.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
1,513件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi JohnDoe1z

it does not support HS200 mode and latest rev.1 Reference Manual (2017)

has not reference to HS200.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,512件の閲覧回数
JohnDoe1z
Contributor III

Thanks! I didn't notice that a new reference manual was released.

I modified the driver to use HS200 and from my first test it was working (SDx_CLK was according to HS200) and the transfer rate from the eMMC also increased by 60%. But it's probably just "luck" that it works...

0 件の賞賛
返信