iMX6DL : LVDS display  pixel jitter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL : LVDS display  pixel jitter

1,703 Views
koichisakagami
Contributor II

Dear community,

 

We face a problem.

 

We lower the i.MX6 core voltage , and
repeat the LVDS output switching(ON/OFF),then
a jitter occurs at the pixel on the LCD display.

 

Why will such a phenomenon occur on i.MX6 ?

The procedure to let a phenomenon reappear with a Sabre board are as follows.

 

[Reproduction Sequence]
   Step1 : Change the core voltage to 1.175v at
                      arch/arm/mach-mx6/mx6q_sabresd_pmic_pfuze100.c
   Step2 : Change the LDB Clock Source  to PLL5 at
                      arch/arm/mach-mx6/clock.c
   Step3 : Change the U-boot environment 
   Step4 : pour  test2.rgb into fb0 in succession 
   Step5 : ON/OFF repeats the fb0 output switch by “blank command” 

 

Then, a jitter occurs at a pixel.
The phenomenon occurs with porbability of 1/10 .
A loupe is necessary to confirm this phenomenon .

 

[System Configurations]
  Board : MCIMX6DL-SDP
  BSP : L3.0.35_4.1.0

 

[STEP1] Change the core voltage to 1.175v

arch/arm/mach-mx6/mx6q_sabresd_pmic_pfuze100.c

Line451
        /*decrease VDDARM_IN/VDDSOC_IN,since we will use ldo bypass mode*/
        /*VDDARM_IN 1.3V*/
        ret = pfuze_reg_rmw(pfuze, PFUZE100_SW1AVOL,
                    PFUZE100_SW1AVOL_VSEL_M,
        //          0x28); // 40d, 1.3V
                    0x23); // 35d, 1.175V
        if (ret)
            goto err;
        /*VDDSOC_IN 1.3V*/
        ret = pfuze_reg_rmw(pfuze, PFUZE100_SW1CVOL,
                    PFUZE100_SW1CVOL_VSEL_M,
    //              0x28);
                    0x23); // 35d, 1.175V

 

[Step2] Change the LDB Clock Source  to PLL5
arch/arm/mach-mx6/clock.c

 

static struct clk ldb_di0_clk = {     
       __INIT_CLK_DEBUG(ldb_di0_clk)    
      .id = 0,    
// .parent = &pll2_pfd_352M,    
     .parent = &pll5_video_main_clk,    
     .enable_reg = MXC_CCM_CCGR3,    
     .enable_shift = MXC_CCM_CCGRx_CG6_OFFSET,  
     .enable = _clk_enable,     
     .disable = _clk_disable,     
     .set_parent = _clk_ldb_di0_set_parent,   
     .set_rate = _clk_ldb_di0_set_rate,    
     .round_rate = _clk_ldb_di_round_rate,   
     .get_rate = _clk_ldb_di0_get_rate,   
     .flags = AHB_HIGH_SET_POINT | CPU_FREQ_TRIG_UPDATE,
};     
     
static struct clk ldb_di1_clk = {     
      __INIT_CLK_DEBUG(ldb_di1_clk)    
     .id = 0,    
// .parent = &pll2_pfd_352M,    
     .parent = &pll5_video_main_clk,    
     .enable_reg = MXC_CCM_CCGR3,    
     .enable_shift = MXC_CCM_CCGRx_CG7_OFFSET,  
     .enable = _clk_enable,     
     .disable = _clk_disable,     
     .set_parent = _clk_ldb_di1_set_parent,   
     .set_rate = _clk_ldb_di1_set_rate,    
     .round_rate = _clk_ldb_di_round_rate,   
     .get_rate = _clk_ldb_di1_get_rate,   
     .flags = AHB_HIGH_SET_POINT | CPU_FREQ_TRIG_UPDATE,
};     
     
//clk_set_parent(&ldb_di0_clk, &pll2_pfd_352M);  
//clk_set_parent(&ldb_di1_clk, &pll2_pfd_352M);  
    clk_set_parent(&ldb_di0_clk, &pll5_video_main_clk); 
    clk_set_parent(&ldb_di1_clk, &pll5_video_main_clk); 

 

[Step3] Change the U-boot environment 

    setenv loadaddr 0x10800000
    setenv bootargs_base 'setenv bootargs console=ttymxc0,115200'
    setenv bootargs_mmc 'setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666,ldb=dul1'
    setenv bootcmd_mmc 'run bootargs_base bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm'
    setenv bootcmd 'run bootcmd_mmc'
    saveenv

 

[Step4] pour  test2.rgb into fb0 in succession 

test2.sh is as follows.

 

#!/bin/sh  
echo "test2.rgb"  
while [ "1" ]  
do  
        cat test2.rgb > /dev/fb0 
done 

 

 

Test2.rgb format is

      [ FF FF FF FF 00 00 00 FF] ……  repeat

116602_116602.pngpastedImage_7.png

      A jitter occurs at this Red pixel

 

I attach the input data file (test2.rgb).

 

 

[Step 5] ON/OFF repeats the fb0 output switch by “blank command” 

 

sh test2.sh &  
echo 1 > /sys/class/graphics/fb0/blank  
echo 0 > /sys/class/graphics/fb0/blank  
[Enter]  
[Enter]  
.......... repeat ............

 

 

 

Best Regards,
Koichi Sakagami

*************************************

Original Attachment has been moved to: test2.rgb.zip

Original Attachment has been moved to: test2.sh

Labels (1)
0 Kudos
Reply
3 Replies

1,277 Views
art
NXP Employee
NXP Employee

As per the clock configuration the customer provided, they have switched the LDB root clock from the PLL2 PFD0 source, whose output frequency is 352MHz, to PLL5 output, whose output frequency is 630MHz. It seems to be too high, since the maximum serializer clock frequency, specified for LDB, is 595MHz. So, please ask the customer to select the clock source with lower frequency for LDB.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,277 Views
koichisakagami
Contributor II

Dear Artur san,

Thank you for your reply.

We will check them.

Best Regards,

Koichi sakagami

0 Kudos
Reply

1,277 Views
koichisakagami
Contributor II

Dear Artur san,

We checked the LDB root clock frequency from PLL5 output.
It was 497.656MHz.

So could you tell us the other way to solve this problem ?

Best Regards,
Koichi Sakagami

0 Kudos
Reply