iMX6DL LPDDR2 Register Programming Aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6DL LPDDR2 Register Programming Aid

Jump to solution
1,744 Views
tom_perman
Contributor III

Can I confirm that the latest available version of iMX6DL register programming aid is v1.3 (linked below)? There was a reference to a version 1.4 in the comments of the linked page

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6DL-LPDDR2-Register-Programming-Aid/...

Labels (1)
0 Kudos
Reply
1 Solution
1,733 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
2 Replies
1,726 Views
tom_perman
Contributor III

Thanks for confirming. 

@TheAdmiral  stated the following error with v1.3 in the linked post: 
"Just found an error in the spreadsheet in the calculation of the nWR value of MR1. Will correct this and add a Pre-Charge all command to the MR programming sequence"

Can you give me more details of this error? Are there any other issues with v1.3 I should be aware of?

Thanks,

 

Tom 

0 Kudos
Reply
1,734 Views
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

0 Kudos
Reply