iMX6DL LPDDR2 Register Programming Aid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6DL LPDDR2 Register Programming Aid

跳至解决方案
1,728 次查看
tom_perman
Contributor III

Can I confirm that the latest available version of iMX6DL register programming aid is v1.3 (linked below)? There was a reference to a version 1.4 in the comments of the linked page

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX6DL-LPDDR2-Register-Programming-Aid/...

标签 (1)
0 项奖励
回复
1 解答
1,717 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,710 次查看
tom_perman
Contributor III

Thanks for confirming. 

@TheAdmiral  stated the following error with v1.3 in the linked post: 
"Just found an error in the spreadsheet in the calculation of the nWR value of MR1. Will correct this and add a Pre-Charge all command to the MR programming sequence"

Can you give me more details of this error? Are there any other issues with v1.3 I should be aware of?

Thanks,

 

Tom 

0 项奖励
回复
1,718 次查看
igorpadykov
NXP Employee
NXP Employee

Hi tom_perman

 

yes latest version of iMX6DL register programming aid is v1.3.

 

Best regards
igor

0 项奖励
回复