iMX6 quad max DDR3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 quad max DDR3

806 Views
wangben
Contributor I

Hi All,

iMX6 Quad supports 4GByte DDR3 at datasheet notes, Can it support to 8GByte?

Labels (1)
0 Kudos
Reply
2 Replies

512 Views
igorpadykov
NXP Employee
NXP Employee

Hi Wang

no, available memory configurations provided in

sect.2.3 DDR mapping to MMDC controller ports IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

512 Views
yangruofei
Contributor I

but i view  Table 6-1. MMDC feature summary , it notice 

Up to 4 Gbyte address space and configurable address space per CS 
Density of 256 Mbytes-8 Gbytes

how can I understand ?

now we use 4GB ddr3 , just connect CS0 .  through  u-boot can recognition 。 but it will be hang when run into kernal uimage.

0 Kudos
Reply