iMX6 quad Mipi display + tear effect/V sync pulse connection?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 quad Mipi display + tear effect/V sync pulse connection?

1,087件の閲覧回数
boulder803
Contributor I

Hi, I wish to use a small 1.54" Mipi display (LH154Q01) with imx6 quad.

I understand the main Mipi connections, clocks & data lanes, but the LH154Q01 display also has a tearing effect / V sync pulse output line - how should this be connected to the imx6 quad?

ラベル(1)
0 件の賞賛
返信
1 返信

892件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Richard

I am afraid i.MX6Q does not have hardware support for LCD

"tearing effect / V sync" input, so one can try to use this LCD without

that signal.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信