iMX6: power-up state of EIM pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6: power-up state of EIM pins

468 Views
alex_t
Contributor I

What is the power-up state of the EIM pins EIM_DA0..EIM_DA15?

We do not use the external bus and would like to use some of these pins as GPIO outputs, but for that we need to know their initial state. I was unable to find anything in the documentation.

The reference shows them mapped to EIM by default. Our boot configuration selects boot from SPI flash. Nothing accesses the EIM during boot. I would expect the pins to remain tri-stated under these circumstances, but it would be nice to have some proof.

 

Labels (2)
0 Kudos
Reply
1 Reply

444 Views
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @alex_t ,

 

Please refer to Chapter 6.2.4 Signals with Different Reset States of datasheet.

Specifically the Table 97. Signals with Differing Before Reset and After Reset States 

Alejandro_Salas_2-1687198122889.png

 

Alejandro_Salas_0-1687198085879.png

Alejandro_Salas_1-1687198101501.png

 

Best regards.

0 Kudos
Reply