iMX6 on-die temperature measurement

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 on-die temperature measurement

1,923件の閲覧回数
jaiganesh
Contributor III

Hello there,

Regarding the thermal management in iMX6, I can see that the bootloader (u-boot) does not allow to boot when the on-die temperature is greater than 80C. The macros used in bootloader are:

#define TEMPERATURE_MIN-40
#define TEMPERATURE_HOT80
#define TEMPERATURE_MAX125

Are these values with respect to commercial iMX6 processors or industrial iMX6 processors?

Thanks,

Jai Ganesh

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,303件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

It is experience value for uboot  application layer. If the temp is great than 85C at uboot stage, normally linux could not run.

0 件の賞賛
返信

1,303件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The value TEMPERATURE_HOT in U-boot is set relatively low for assurance,

in order to avoid overheat issues. Note, the accuracy of the sensor is not high

(~10 degree). 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信