Hi! We have a device using an iMX6 with Dunfell and are porting it to Yocto Kirkstone. We want to keep using SecureBoot/HAB on it. By looking at a recent u-boot's code [0] it would be a matter of enabling CONFIG_IMX_HAB... except it fails to build pretty quickly:
git/arch/arm/mach-imx/hab.c:875: undefined reference to `fuse_read'
And indeed the fuse_read() function seems to be only defined for iMX8, even if the doc says this should be supported from iMX6 to 8.
Older instructions for enabling this talk about CONFIG_SECURE_BOOT, which does not seems to exist anymore on u-boot.
So, what's the correct way to enable HAB on iMX6? A solution using u-boot-imx is just fine.
[0] I used 2022.04 as a starting point, but I see the same issue on 2023.04.
已解决! 转到解答。
Thanks to the u-boot people the root issue has been found.
CONFIG_SPL_DRIVERS_MISC=y
↑ This was also needed, and should probably be selected by CONFIG_IMX_HAB=y.
Thanks to the u-boot people the root issue has been found.
CONFIG_SPL_DRIVERS_MISC=y
↑ This was also needed, and should probably be selected by CONFIG_IMX_HAB=y.
Hello,
Have no try this for MX6 but it should works:
Regards
Thanks, but that will not work. Check that the first thing to do is to enable CONFIG_SECURE_BOOT. But now:
$ git clone https://github.com/nxp-imx/uboot-imx.git
$ cd uboot-imx/0
$ git branch
* lf_v2022.04
$ grep -Rn CONFIG_SECURE_BOOT
$
So that does not seems to be an option any more.