iMX6 install error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,203件の閲覧回数
xuankong
Contributor II


I am trying to install LTIB for my I.MX6 SoloLite board. I am using Ubuntu 12.04 LTS. I have downloaded the file titled “L3.0.35_12.10.02_ER_SOURCE" and installed the dependencies as well as patched LTIB. I am stuck when running the LTIB. The log file says:

Processing: wget
==================

Build path taken because: directory build, no prebuilt rpm,

Cowardly refusing to clobber existing directory:
/opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1
Remove this by hand if you really want to rebuild this package from scratch

Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
main::host_checks:1447
main:554

I tried to fix it by remove wget -1.9.1 by hand and rebuiled this package from scratch. BUT a NEW problem occurs.

The log file shows:

Processing: wget

==================

Build path taken because: no prebuilt rpm,

….

make[1]: *** [wget] Error 1
make[1]: Leaving directory `/opt/freescale/ltib/usr/src/rpm/BUILD/wget-1.9.1/src'
make: *** [src] Error 2
error: Bad exit status from /home/kongxuan/Documents/imx6install/ltib/tmp/rpm-tmp.57542 (%build)

RPM build errors:
    Bad exit status from /home/kongxuan/Documents/imx6install/ltib/tmp/rpm-tmp.57542 (%build)
Build time for wget: 16 seconds

Failed building wget
Died at ./ltib line 1392.
traceback:
main::build_host_rpms:1392
  main::host_checks:1447
   main:554

It seems that I did not have wget rpm package. I attached my log file here.

Please help me to solve the problem !

Thanks !

Original Attachment has been moved to: host_config.log.zip

0 件の賞賛
返信
1 解決策
1,833件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You can google the wget -1.9.1 source code and then download it and store it to the /opt/freescale/pkgs/.

./ltib -p wget -m prep  (extract the source code to rpm/BUILD/)

./ltib -p wget -m scbuild (rebuild the source code)

./ltib -p wget -m scdeploy (install to the rootfs)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,834件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You can google the wget -1.9.1 source code and then download it and store it to the /opt/freescale/pkgs/.

./ltib -p wget -m prep  (extract the source code to rpm/BUILD/)

./ltib -p wget -m scbuild (rebuild the source code)

./ltib -p wget -m scdeploy (install to the rootfs)

0 件の賞賛
返信