iMX6 framebuffer error with yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMX6 framebuffer error with yocto

ソリューションへジャンプ
2,798件の閲覧回数
krisztianbakos
Contributor II

Hello,

I have a strange error with my custom iMX6 board, running Yocto -> fido | meta-qt5 -> fido.

The framebuffer device comes up and I see picture on my LCD screen, but after some minutes I get the following error:

root@imx6qsabresd:~# imx-ipuv3 2400000.ipu: ch = 9, pm_runtime_put failed:-38!

CPU: 0 PID: 25 Comm: kworker/0:1 Not tainted 3.14.28-1.0.0_ga+g91cf351 #7

Workqueue: events console_callback

[<80014644>] (unwind_backtrace) from [<8001164c>] (show_stack+0x10/0x14)

[<8001164c>] (show_stack) from [<8065485c>] (dump_stack+0x7c/0xbc)

[<8065485c>] (dump_stack) from [<80459cdc>] (ipu_uninit_channel+0x524/0xa7c)

[<80459cdc>] (ipu_uninit_channel) from [<802ca220>] (mxcfb_blank+0x80/0xb8)

[<802ca220>] (mxcfb_blank) from [<802b0550>] (fb_blank+0x54/0xa8)

[<802b0550>] (fb_blank) from [<802ba92c>] (fbcon_blank+0xf4/0x2a8)

[<802ba92c>] (fbcon_blank) from [<802f6604>] (do_blank_screen+0x1d4/0x284)

[<802f6604>] (do_blank_screen) from [<802f94dc>] (console_callback+0x88/0x15c)

[<802f94dc>] (console_callback) from [<8003ed2c>] (process_one_work+0xf4/0x35c)

[<8003ed2c>] (process_one_work) from [<8003f97c>] (worker_thread+0x130/0x3bc)

[<8003f97c>] (worker_thread) from [<80044c3c>] (kthread+0xcc/0xe4)

[<80044c3c>] (kthread) from [<8000e478>] (ret_from_fork+0x14/0x3c)

And my screen goes off (pixel clock stops)

Does anyone have any idea what could be the problem?

Thank you in advance!

Best regards,

Krisztián Bakos

ラベル(4)
0 件の賞賛
返信
1 解決策
2,481件の閲覧回数
krisztianbakos
Contributor II

Hello Alfred,

Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')

Best Regards,

Krisztián

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,481件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Krisztian,

It looks like you are getting some external exception and it is not handle correctly, you can check your dtsi files, for the default_ifmt and the pinctrl.

Hope this helps

0 件の賞賛
返信
2,482件の閲覧回数
krisztianbakos
Contributor II

Hello Alfred,

Thank you for the answer. The thing is, that the power management was disabled in the Kernel, thus it could not switch power states. I re-enabled it and now it works fine. However, this was not such a huge issue as I could re-enable the screen (turned out it was the "screensaver"... -.-')

Best Regards,

Krisztián

0 件の賞賛
返信