iMX6 custom uboot with mfg tool v2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 custom uboot with mfg tool v2

771 Views
J_W
Contributor III

Hi,

I've been trying to wrap my head around the MFG tool as I need to configure a GPIO to flash my device. My issue is that I cannot use the standard intermediate u-boot because my device will simply power down if a GPIO is not properly configured. There seem to be so many different versions of U-boot - I am not sure what I am supposed to do. Looking in my ucl2.xml file I can see that the first u-boot that is loaded on the device is 

<CMD state="BootStrap" type="boot" body="Recovery" file="../../TX6_MFG/u-boot_mfg.bin" >Loading mfg U-Boot...</CMD>

I assume that this is the one that I need to replace? Where would I be able to find the source code for u-boot_mfg.bin? 

This is an old version of the Freescale MFG Tool V2 2.1.0. 

0 Kudos
Reply
0 Replies