iMX6 and Marvell switch 88E6060 multiple ports detect.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 and Marvell switch 88E6060 multiple ports detect.

1,703 Views
shu-kangtseng
Contributor I

Hi,

I have a custom board that use iMX6-Dual lite as CPU.

The board has a Marvell switch 88E6060.

The Linux kernel version is 3.0.35 that got from LTIB L3.0.35_4.1.0.

I changed to RMII by refer https://community.freescale.com/servlet/JiveServlet/download/398432-274101/MX6_enet_RMII.zip

The Ethernet driver of L3.0.35_4.1.0 designed for single Ethernet PHY.

I only see "Link is Up" message when Ethernet cable connect to port 0 of switch,

I can’t see "Link is Up" message when Ethernet cable connect to other ports.

The problem is Ethernet driver only detect port 0.

Is there any patch that let Ethernet link up when connect any port?

Thank you very much.

  -Jason

0 Kudos
1 Reply

559 Views
art
NXP Employee
NXP Employee

The most likely cause of the issue is that the switch requires some additional configuration to make all of the ports (not only Port 0) functional after power-up. You can check it with the switch vendor.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos