iMX6 SoloX: Frequency limitation for industrial variant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX6 SoloX: Frequency limitation for industrial variant

661 Views
peder_alm
Contributor I

What is the technical limitation for the iMX6 SoloX regarding CPU frequency for the industrial variant? The Commercial variant can run in 1GHz, but only in 800MHz for the industrial variant. Why is that? My source for this is the following documents:

i.MX 6SoloX Applications Processors for Industrial Products - Data Sheet (REV 4)

i.MX 6SoloX Applications Processors for Consumer Products - Data Sheet (REV 4)

pastedImage_1.png

pastedImage_2.png

Labels (1)
0 Kudos
3 Replies

566 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peder

differencies are defined in factory testing, industrial parts are -40 to
+105°C while commercial -20 to +105°C. Also some differencies can be found in

i.MX 6SoloX Product Lifetime Usage Estimates - Application Notes

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

566 Views
peder_alm
Contributor I

So there is no hardware limitations? I can run it in any frequency defined in imx6sx.dtsi if I like to?

0 Kudos

566 Views
igorpadykov
NXP Employee
NXP Employee

right. Provided that operating frequency does not exceed datasheet values.

0 Kudos