What is the technical limitation for the iMX6 SoloX regarding CPU frequency for the industrial variant? The Commercial variant can run in 1GHz, but only in 800MHz for the industrial variant. Why is that? My source for this is the following documents:
i.MX 6SoloX Applications Processors for Industrial Products - Data Sheet (REV 4)
i.MX 6SoloX Applications Processors for Consumer Products - Data Sheet (REV 4)
Hi Peder
differencies are defined in factory testing, industrial parts are -40 to
+105°C while commercial -20 to +105°C. Also some differencies can be found in
i.MX 6SoloX Product Lifetime Usage Estimates - Application Notes
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
So there is no hardware limitations? I can run it in any frequency defined in imx6sx.dtsi if I like to?
right. Provided that operating frequency does not exceed datasheet values.