iMX6 SoloLite EVK BOM does not have MFGPN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

iMX6 SoloLite EVK BOM does not have MFGPN

346 次查看
kristinp
Contributor I

Hi, I'm trying to attach a CMOS sensor to the iMX6 Sololite EVK and need to create a jumper board to interface between my sensor and the EVK. However, when I download the BOM, there is no field for Manufacturing Pin Number, so I am not sure what type of connector the kit is using. Could you provide a BOM with the MPN of all the components in a CSV, text or Excel format?

Thank you!

标签 (1)
标记 (3)
0 项奖励
1 回复

312 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Kristin

please create service request :
https://community.freescale.com/docs/DOC-329745

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励