Hi,
We are trying to access iMX6 S/DL SDMA from a EIM FPGA . The SDMA scheduler SDMA_event_0 always detects a rising edge. Is there a way to change this to detect falling edge using any register settings or the HW is always designed in a way only to detect rising edge. Thanks
解決済! 解決策の投稿を見る。
Hi Raajesh
I am afraid SDMA_event_0 detection polarity can not be changed as
it is fixed in hardware, sorry.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Can we use SDMA_EVENT_0 to trigger events. We are abe to use only EVENT_1. Kindly help to clarify.Thanks
Hi Raajesh
seems not as Table 3-2. SDMA event mapping describes only EVENT_1
Best regards
igor
Hi Igor,
Thanks, could you please help on the procedure to use EVENT0 as well if any.
Regards,
Raajesh K
Hi Raajesh
this is not "officially supported", means no support is described in
Linux Release Notes included in Linux documentation:
i.MX Software and Development Tools | NXP
Standard support path in such cases: Commercial Support and Engineering Services | NXP
Best regards
igor
Hi Igor,
Thanks for the support. Will proceed accordingly.
Regards,
Raajesh K
Hi Raajesh
I am afraid SDMA_event_0 detection polarity can not be changed as
it is fixed in hardware, sorry.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
We are facing one more issue with SDMA event. Even though we configure to use SDMA_EVENT_0 as interupt the SDMA is triggered only when EVENT_1 is triggered. I saw there is something related to SOC revision in one of the NXP forum discussion https://community.nxp.com/thread/324491 . Is this is the case? If so can you specify the revisions for Quad and Solo/Dual. Thanks
Regards,
Raajesh K
Hi Raajesh
as answered on that link, there are no SDMA_event_0 scripts, so you
will have to write new script for it. I am afraid that info about revisions
is not available regarding SDMA_EVENT.
Best regards
igor
Hi Igor,
So it means we can use only EVENT_1 to trigger SDMA requests. Is my understanding correct. Thanks
Regards,
Raajesh K
Hi Igor,
Is my understanding correct? Thanks
Hi Igor,
Thanks for the confirmation.
Regards,
Raajesh K