iMX6 Reference manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

iMX6 Reference manual

跳至解决方案
2,470 次查看
xiongweihuang
Contributor III

Hello all

I get reading from

Document Number: IMX6DQRM  Rev. 1, 04/2013 @ Page 2696

• RGB565 over 16 bit = 2 cycles/pixel

As I understand , RGB565 is take 16bit in ram , and all dma transfer can finished in 1 clock with paral data , Why this takes 2 cycles ?

While At the same page

• RGB888 over 8 bit = 3 cycles/pixel

This is fiexed from Document Number: IMX6DQRM Rev. 0, 11/2012 @Page 2671

This is  a little wired , I dont know if your chip will have some special trick for dma transfer ? high dma data transfer limit ?

But at same page

• YUV422 over 16 bit = 1 cycles/pixel

Or , just Document error ?

Regards

0 项奖励
回复
1 解答
1,895 次查看
Yuri
NXP Employee
NXP Employee

Yes, this is a misprint : RGB565 over 16 bit requires  1 cycle/pixel


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,896 次查看
Yuri
NXP Employee
NXP Employee

Yes, this is a misprint : RGB565 over 16 bit requires  1 cycle/pixel


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复